This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to scale the 5M or 10M image to 1080P in DM8127 IPNC RDK?



Hello!

I purchased a DM8127 IPNC from Appro,and use the V3.5 version RDK to develop a IPC.

I want to use the 10MP/5MP MJPEG+1080P H.264 dualstream usercase in my application, and I design the pipeline based on tristream lowper usercase.but I find I can't get the second HD stream(means biggger than 1080P) from the camera link,the second outstream can't be set to 1080P resolution.so I try to add a ISP or scalar link after the 10MP stream,and still can't get correct result?

so My qustion is:How can I resize the 10M or 5M resolution image to 1080P resolution?what is the framerate?

Thank you very much.

btw:

I find the isp link can't output more higher resolution than 1920x1080.if I set the output resolutuon to be 5M,the isp link create process will failed at memery allocation.so I think I should change the memory allocation table.but how can I do it?is there any other methods to do this?
thank you!