This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3EVM SDK_1.0.2 Framebuffer resolution on DVI



Hi,

I'm trying to get DVI output with XGA resolution.

I added XGA code to arch/arm/plat-omap/display.c in SDK_1.0.2 kernel. As per instruction here: http://wiki.davincidsp.com/index.php?title=Adding_new_DVI_resolutions

Entered this into console:

echo DVI > /sys/class/display_control/omap_disp_control/ch0_output
echo XGA > /sys/class/display_control/omap_disp_control/ch0_mode

I got the output to the external display. The display sees the mode as being 1024x768 70Hz, but I only see the picture (blue screen that is) occupying roughly one half of the screen -- it reaches about the half of the screen from left to right, and doesn't reach to the bottom.

My assumption is that the frambuffer resolution is not set correctly. I tried issuing fbset command, that is part of the busybox

fbset -fb /dev/fb0 -xres 1024 -yres 768

No change. When I issue it with no arguments, it tells me

mode "480x640-145"

...

Can anyone give me a hint on what's happening here and how I get things to work full screen with XGA.

Thanks!