Hi Champs,
#1:
We are designing Board with DM8168 which has small size PCB.
I have to avoid discrete as much as possible. We will be using SD Card Boot for DM8168 (BTMODE[4:0] = 10111 )
BTMODE3 will be routed out from BGA and i will add external Pull Down to it.
BTMODE0, BTMODE1, BTMODE2, BTMODE4 wont be routed out from BGA and i wont add any external termination to them.
Also, CS0BW, CS0MUX[1], CS0MUX[0], CS0WAIT wont be routed out from BGA and i wont add any external termination to them.
#2:
EMAC[1] is not used in our design.
EMAC[1]_COL, EMAC[1]_RXER, EMAC[1]_TXCLK can i keep these pins open?
Since these pins are marked as "PULL: IPD / DIS" which means, no internal termination after Reset.
#3:
NMI (External active low maskable interrupt) is not used in our design.
can i avoid External Pullup termination and keep this pin open?
Best Regards
Feroz