Hi
I have a question about the pinmux for mmc1 (use for BBB)
In the TI utility there is for example this possibility : mmc1_dat0_mux2 under MODE1 on ball U7 (first line on the sheet). Am I correct that this pin has to be programmed as mode 1 in the corresponding pinmux register , being GPMC_AD0) . If so (or not) , then wat does this mux2 mean ??? Is there some other register to be programmed that represents this mux2 value ? What exactly is this mux2 ?
Kind regards ,
Ronny