One of my hardware engineers asks:
"We are having variable success getting SRAM. The 166MHz ISSI part seems to be unobtainable right now. There is a 140MHZ ISSI part with some lead time. There is a 133MHZ Micron part that is available. I know if I plug into my PC any speed of RAM the bios will check the part and run it automatically at the speed it was designed for (unless I overclock it). Do you know if the software you are using will operate the SRAM at the designed frequency automatically?"
I don't know the answer and I'm hoping one of you can tell me. If it isn't "automatic", what file do I change to add the wait states?