Hi,
We are trying to boot AM3352 using NOR flash(Non-muxed) in "Fast External Booting" mode SYSBOOT[4:0]=11111b .
The TRM manual says "in this mode the device is connected in XIP_MUX1 configuration",
but in our case the ROM Code seems like trying to access the "XIP_MUX2" pins.
During the boot process we see changes in the LCD_DATAx pins(Pin used for XIP_MUX2 mode)
instead of changes in GPMC_Ax pins as in XIP_MUX1 mode.
Please let me know is there is any settings to be considered with Fast External Booting.
Best Regards
Prad