Hi all,
I am running the dsplink readwrite example and I am getting the error message below. I have read the platformguide_omap3530 as well as this wiki http://wiki.davincidsp.com/index.php?title=DSP_MMU_Faults#If_you_know_the_memory_range_to_map_to_the_DSP_MMU_at_build_time_of_DSP_server
but I am still having difficulty figuring out what is going on.
I am running Linux on the ARM and not using LPM nor CMEM. Should I enable hardware TWL to resolve this?
Another odd thing is the .out file used to work fine but now it is giving me this error.
============= Sample Application : READWRITE ==========
Entered RDWR_Create ()
Leaving RDWR_Create ()DSP MMU Error Fault! MMU_IRQSTATUS = [0x1]. Virtual DSP addr reference that generated the interrupt = [0xff204100].