According to the Linux Cryptography User's Guide, I should be able to configure the Hardware Random Number Generator (HWRNG) as a character device in my kernel. However, I don't have that option. Furthermore, I don't see the OMAP4 HWRNG option. I'm using kernel 3.8.13-bone26.
Is there a patch that I can apply to enable this?
I've other posts on these forums requesting additional information for the crypto / HWRNG specs. I'm submitting patches to OpenSSL to increase the availability of the algorithms for the linux-crypto dev driver. Can I receive access to these documents to help improve the open source tools?
Thanks,
Josh