Other Parts Discussed in Thread: DM3730, OMAP3530
I have followed the instructions for changing the memory mapping of Linux and the DSP found at http://processors.wiki.ti.com/index.php/Changing_DSPLink_Memory_Map
My ARM side app and DSP app are running fine except that the I can no longer get my buffers transferred back and forth using DSPLink (specifically ring_io). This was working fine before I changed the memory addresses. Interestingly, I can still print DSP app debug traces on the ARM side app, so I believe I at least have the addressing setup correctly for the ARM and DSP applications.
I have changed the allocation to be 256M for ARM and 256M for DSP on my Gumstix Overo IronStorm (DM3730).
Here is an excerpt from dsplink-omap3530-base.tci
…
prog.module("GBL").C64PLUSMAR128to159 = 0x1FFF0000 ;/* Make sure DSPLINKMEM segment is NOT cached */
…
/* ============================================================================
* MEM : RESET_VECTOR
* ============================================================================
*/
var RESET_VECTOR = prog.module("MEM").create("RESET_VECTOR");
RESET_VECTOR.base = 0x90000000 ;
RESET_VECTOR.len = 0x00000080;
RESET_VECTOR.space = "code/data";
RESET_VECTOR.createHeap = false;
RESET_VECTOR.comment = "RESET_VECTOR";
/* ============================================================================
* MEM : Adjust DDR2
* ============================================================================
*/
var DDR2 = prog.module("MEM").instance("DDR2");
DDR2.base = RESET_VECTOR.base + RESET_VECTOR.len ;
DDR2.len = 0x8FFFF80;
DDR2.space = "code/data";
DDR2.createHeap = true;
DDR2.heapSize = 0x8000000;
DDR2.comment = "DDR2";
/* ============================================================================
* MEM : DSPLINKMEM
* ============================================================================
*/
var DSPLINKMEM = prog.module("MEM").create("DSPLINKMEM");
DSPLINKMEM.base = DDR2.base + DDR2.len ;
DSPLINKMEM.len = 0x00030000;
DSPLINKMEM.createHeap = false;
DSPLINKMEM.comment = "DSPLINKMEM";
/* ============================================================================
* MEM : DSPLINKMEM
* ============================================================================
*/
var POOLMEM = prog.module("MEM").create("POOLMEM");
POOLMEM.base = DSPLINKMEM.base + DSPLINKMEM.len ;
POOLMEM.len = 0xD0000;
POOLMEM.createHeap = false;
POOLMEM.comment = "POOLMEM";
Here is an excerpt from CFG_OMAP3530_SHMEM.c
#define RSTENTRYID 0u
#define RESETCTRLADDR 0x90000000u
#define RESETCTRLSIZE 0x80u
#define CODEENTRYID 1u
#define CODEMEMORYADDR (RESETCTRLADDR + RESETCTRLSIZE)
#define CODEMEMORYSIZE 0x8FFFF80u
#define SHAREDENTRYID0 2u
#define SHAREDMEMORYADDR0 (CODEMEMORYADDR + CODEMEMORYSIZE)
#define SHAREDMEMORYSIZE0 0x5000u
#define SHAREDENTRYID1 3u
#define SHAREDMEMORYADDR1 (SHAREDMEMORYADDR0 + SHAREDMEMORYSIZE0)
#define SHAREDMEMORYSIZE1 0x2B000u
#define POOLENTRYID 4u
#define POOLMEMORYADDR (SHAREDMEMORYADDR1 + SHAREDMEMORYSIZE1)
#define POOLMEMORYSIZE 0x000D0000u