This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash Player on omap3503 and web browsing

Other Parts Discussed in Thread: OMAP3530

I have seen the interesting news some days ago,
http://focus.ti.com/pr/docs/preldetail.tsp?sectionId=594&prelId=sc09045   .
that is about an Adobe Flash 10 player working, in beta realease, for the second half of 2009, and stable version for Q1 2010.
But all developers tell me that the cpu resources could not be enough to run flash on omap3530/03 at 600Mhz.
I'd like to see, as soon as possible, some alpha releases and its platform requirements, I mean how much RAM, and which libraries I need to have in my distro.
Adobe Flash player will be in binary version, so it has to find a compatible distro.
I know there are commmercial solutions for flash lite and opensource flash players, but they are not fully compatible with flash 10.

Moreover this flash player will have to work as a web browser plugin, but by now the best browser I tried on omap3530/03 is firefox 3.0.1, with its heavy cpu request that is about 60% and more.

So I don't understand which is the best distro that will drive in the future the Linux OMAP based notebook.
Looking this link:
http://www.linuxdevices.com/news/NS9022878225.html?kc=rss
seems that the touchbook, with openembedded/Angstrom with fennec mozilla browser, could be the solution.
But I hear rumours about problems of fennec browser cpu usage.
I don't know also if fennec is really functional as firefox or is still limited.

Anybody can put in me in the right direction?

Thank you very much in advance,
Recalcati