This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unstable bitrate while changing bitrate dynamically



Hello TI,

We are using DM8148 based custom board and using ezsdk_dm814x-evm_5_05_01_04 from software perspective.

In one of our application it is required to change bit-rate dynamically which we achieve successfully, but when we change bitrate dynamically, bit-rate is not stable. For example, we set initial target bitrate to 200 kbps and the actual corresponding bitrate is accurate (equal to 205-210 kbps). However, after switching target bitrate to 600 kbps the actual encoder output bit-rate is approximately 450 kbps.

we attached video sample here with the 600 kbps bitrate after 100 frames of video for your reference.

8156.7181.sample.rar

Please suggest.

Thanks,

Devang