Hi,
I have a customer that is having a hard time getting his 6678 connect to an SGMII-GMII bridge (Max24288). They are using an example from TI’s PDK package, namely the “pdk_C6678_1_1_2_6_old\packages\ti\drv\exampleProjects\PA_emacExample_exampleProject”, to configure the SGMII interface of the 6678. The example was modified to use the SGMII 0 port instead of SGMII 1. That is pretty much the only difference from the original source from TI. However:
- They are able to perform both internal SGMII and SERDES loopbacks within the DSP but not outside the DSP.
- They are able to perform GMII loopbacks within the MAX24288 chip.
- They cannot get any traffic to pass from the TI DSP (SGMII) to the SGMII interface chip (MAX24288).
I consulted the doc recommended (on post #104726: http://www.ti.com/lit/ug/sprugv9b/sprugv9b.pdf) but I don't see anything that could help; However I could not figure out if the 6678 expected the interface chip to be in SGMII master or Slave mode?
Could you possibly have someone review the SGMII port 1 to SGMII port 0 change that my customer did on the TI example code please? You might have some suggestions to make this work.
Please advise as I need help on this issue badly.
Thanks
Electrons4me