Other Parts Discussed in Thread: TVP5158
Hi,
I'm using 814x with DVRRDK McFW demo example,
I modified the example to display image(capture from tvp5158) to QVGA(320x240) LCD(via DVO2),
the result like the following pictures.
the output resolution seems correct(as 4ch mode via swms link),
but the image will be shift(both vertical and horizontal) and twinkling,
i guess it's Hsync, Vsync issue like polarity, timing or pulse width,
but it doesn't work when i change the config.
any suggestions? thanks.