Hi,
I have a question about C6670 SPI boot.
In our custom board, it boots up from SPI NOR Flash.
If all code and data is loaded to L2SRAM, it boots with no problem.
But if all code/data is loaded to DDR3, boot will be done but the code/data in DDR3 is incorrect.
I made a DDR configuration table as following E2E:
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/288354/1012614.aspx#1012614
After boot, I checked the DDR3 Memory Controller Registers from CCS Memory Browser
and it was set correctly. But it
I guess that DDR configuration table's parameter is not enough for initializing DDR3.
Isn't DDR3 Configuration Register 0 to 24 need to be initialized during RBL?
If it is true, how to configure it? It seem there is no examples and documentation.
Please give me an advice and information.
best regards,
g.f.