Other Parts Discussed in Thread: TPS65920, OMAP3530
Scanning through the OMAP3 documentation I can't find what the state definitions of the JTAG_EMU0 and JTAG_EMU1 pins mean. I have compared the pins on the Mistral EVM and on the Beagleboard. The Mistral EVM has a dip switch for both the EMU0 and EMU1 which allows the user to "enable the JTAG" when the EMU0 pin is pulled Low(switch on) and when the EMU0 pin is High(switch off) the "JTAG is disabled". On the Beagleboard this pull down or jumper on the EMU0 pin has been removed but it claims you can still use the JTAG connector for debugging the OMAP3. So I don't quite understand what happens when EMU0 is low or high?
In our design I would like to use the JTAG interface for both OMAP3 debugging, just peeking and poking using the XDS510 emulator as I know it's not OS aware, and also use the JTAG interface for Boundary Scan on the OMAP3. I would like to also have the TPS65920 on the JTAG chain. Do you see any problems with the TPS65920 on the same JTAG chain as the OMAP3?
Thanks for your help,
Gary