This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Raw Image capture ducati



Hi

 Using SW release 4AJ.2.2  for OMAP4460 ,8830 sensor .

  We are   capturing  10 bit raw  Bayer image (PIXEL_FORAT_BAYER_RGGB) data using camera_test -f  ,but issue is the captured image file is having only 75% data and rest all are zero.other formats are image data is complete.

 We found buffers received from ducati at OMXCameradapter layer is containing only 75% data for RAW captured image .

Is there any issue with 4AJ.2.2 ducati release  for capturing bayer raw data ?

Any pointers or suggesions for getting complete 10 bit RAW BAYER  data completely