This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EDMA in the DSP side codec..

Hi,

I need to do EDMA in the DSP side codec using the DMAN3 interface.

I have tried going through the documents which tell that DMAN3 should be used to do EDMA3.

Please suggest me the best way. An example would be helpful.

I have gone thru the edma_codec1 example in the Framework components example.
But could not understand it well.

Also in the wiki article, it was mentioned to use IRES interface to configure the EDMA3
If we want to access the DMAN3 APIs for the codec, do I need to create a seperate library for EDMA3?
If so can you suggest me some example?

Thanks and Regards,

Suresh Kumar CV