This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 Reset and Initialization

6657  initialization requires 500 SYSCLK1 periods after the Power Stabilization Phase. The maximum clock period is 33.33 nsec so a delay of an additional 16 μs is required before a rising edge of POR

During the 16 μs ,RBL take over the initialization  ?  i though the RBL execute after the POR and RESETFULL signal released , so why   a delay of an additional 16 μs is required before a rising edge of POR   

Can you describe the initialization step  clearly

  • The clock is required before the reset is released to ensure that the reset has propagated through the part and everything is completely initialized. Once this occurs then the release of the reset will initiate the execution of the Rom Bootloader.

    Regards, Bill