Hi,
I have a question regarding the mapping of the AxC samples in 20 MHz LTE configuration of CPRI protocol using AIF2.
From Chapter 3 of the AIF2 user guide I have read that for 20MHz LTE case for a 4x rate link has eight samples of antenna 0 (AxC0) followed by eight samples of AxC1. However I need to implement a different mapping for the AxC, where every sample of antenna 0 is followed by a sample of antenna 1. I have seen such a case in the document "AIF1-to-AIF2 Antenna Interface Migration Guide" in the Transmission Rule Setup Example of CPRI (page 21 of 36) which is said to use parameter X = 2.
I would like someone to clarify two things for me, first of all; am I getting the correct idea from the figure in the document "AIF1-to-AIF2 Antenna Interface Migration Guide"? Is it really possible to change the mapping by changing only the X value, supposedly the DBMX value of linkconfig? If not how can I switch my CPRI LTE AxC mapping to the indicated configuration by changing the PE and PD parameters?
Thanks in advance,
ilke