Dear all,
my software is dvsdk4.02, dmai_2_20_00_15.
my input yuv is 1280x720 but I just want to encoder the left half part, so I setting :
dynParams.inputWidth = 640; /left half
dynParams.inputHeight = 720;
dynParams.captureWidth = 1280; //line length
Ienc1_create(hEngine, args->codecName, ¶ms, &dynParams);
Ienc1_create will fail and the encStatus.extendedError is 0x0000c00a, which means "Error in capture width parameter".
How can I do this? Is this means I must use edma to copy it before encoder?
Best Regards, 姜 维