Other Parts Discussed in Thread: LM10010, LM10011
hello,everybody,I came cross a question .so,I have several questions.
1,how much is the power consumption of c6678.
2.the full load current of the power is 15A, output voltage is 1V, The output power is 15w, the power can supply c6678?the full load current of the other power is 25A, output voltage is 1V,this power can supply ?
3. the question that I came cross is that when c6678 operate full load,the two powers both shut down suddenly.
I do not know what happened?