Hello all,
We have with us a 2430 SDP. We had been using on the ARM core till now. We had linux running on the ARM core.
- CASE1
We wanted to use the DSP core alone now (No ARM). We wanted to check how to connect to the DSP core. Is there a seperate Boot loader which needs to be loaded for this case ?
Or we just leave the linux to boot on the ARM core and the ARM will also boot the DSP core too. And we could connect the board using XDS 560 (Spectrum digital) and use CCS to connect to the board and download the program. ?
So, basically, what is the procedure to be used, while using only the DSP core.
- CASE2
And also, the procedure to be used to connect to the board, if we want to connect to the DSP core while having Linux on the ARM core ? And use the bridge to communicate between ARM and DSP.
Kindly let me know if any information is required.
thanks and regards
prasanna