Hi All,
I am trying to understand the booting flow in OMAP3530. When i switch on the board U boot Prompt comes up on the Hyperterminal.
Where is the PC pointed just after the switch on.? Is it 0x0 ?
Execution begins with X-loader. Where is x-loader residing? Can you brief me the booting procedure till the point from where the u-boot comes up. ?
When u boot is executed does it automatically run all its diagnostic test (ITBOK) or do we need to run it separately once u-boot prompts come up?
Please help
Jack