Other Parts Discussed in Thread: OMAP3530
The README for the latest x-loader (from OMAP 35x EVM SDK 1.0.2) states that x-loader was modified in Dec. 2006 to support 3430SDP board. Was it ever modified to specifically support the 3530 EVM board, and if so, is that version of x-loader available? The code only seems to reference 34xx variants, and no 35xx variants.
The same questions apply to the u-boot code. Was it ever specifically modified to support the 3530 EVM?
This makes me wonder if I should use SDK x-loader + u-boot or look to use something more up-to-date for 35xx like maybe omap zoom git? Any suggestions?
My hardware is based on OMAP 35x EVM, but I'd like to get latest support for 3530 as possible.
Thanks