This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

building Android issues

I am trying to build the Android ICS filesystem for the BeagleBoard-xm and I have been running into the following issue:

frameworks/base/include/utils/KeyedVector.h:193:31: error: ‘indexOfKey’ was not declared in this scope, and no declarations were found by argument-dependent lookup at the point of instantiation [-fpermissive]
frameworks/base/include/utils/KeyedVector.h:193:31: note: declarations in dependent base ‘android::KeyedVector<android::String8, android::sp<AaptDir> >’ are not found by unqualified lookup
frameworks/base/include/utils/KeyedVector.h:193:31: note: use ‘this->indexOfKey’ instead
make: *** [out/host/linux-x86/obj/EXECUTABLES/aapt_intermediates/AaptAssets.o] Error 1

The x-loader, u-boot, and kernel are built correctly but this is failing. I got the source from the rowboat repo using the link in the TI-Android-ICS-4.0.3-DevKit-3.0.0_DevelopersGuide found here:

http://processors.wiki.ti.com/index.php/TI-Android-ICS-4.0.3-DevKit-3.0.0_DevelopersGuide#Build_Procedure

I am using Ubuntu 12.04LTS and I installed all of the needed packages as recommended by the google android initialization site.

Any help is greatly appreciated