This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP3530] Implementaion of DMAN3



Hi All

  I am new to DMA frameworks.

1. In fastcopy example they are calling the ALG_create , but the function def is not there, from wher it is get?

     should i include the alg_create.c.

2. which file should i add ,so that to get the number of dma channels from the library(dmaGetChannelCnt). i am bit confusing b/w mem model and dman3.

3.Im not able to run the fastcopy .pjt  on hardware,it is hanging near ALG_create , please tell me the sugessions.

Thanks in advance

sureshkumar