This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MIstral EVM 3503 and CCS

Other Parts Discussed in Thread: OMAP3530helo, please help to resolve my problems with Mistral EVM 3503 board I can't connect DSP side using CCS. Besides, ARM side is working perfectly. Even, I have managed to compile and start simple programs. CCS version - 3.3 >R9 Setup file: OMAP3530 XDS510 Emulator DSP : C6400PLUS_0 Error Message: The target does not have a CPU clock. In summer of 2008, TI guys told me that all EVM boardshas the same chip called from then Omap 35x, thus it follows that has full functionality. Please help me to answer the following questions: Is is possible to use DSP side on Mistral EVM 3503 board. If so, how to configure CCS setup ? is there a document with description? Is there a document where is described how to build a multicore application(arm and dsp working independently, with interprocessor protocol) Is there a possibility to build multicore application on pure linux machine without CCS? Sincerely, Mihail