Other Parts Discussed in Thread: OMAP3530
Hi All
I am presently working on omap3530, to fit in to codec engine i allready made the code(H264decoder) as xdm compliance and it is giving bit exactness in ccs. but i put in same lib in codec engine it is hanging while when i run the code.
what would be the problem?
1. Presently i am running the application and library in ccs dsp window. my doubt is application is to be run in arm window present in ccs?
2. in codec engine it is asking *.av5t library how do i generate this library in ccs?
3 If i want to fit our library in to codec engine , some modifications to be done in codec engine side ,please tell me wher should i changes to be made. is there any artical or docs.
Thanks in advance
suresh