I am trying to find out what hardware and software is required to support SVGA (800x600) resolution using RGB signaling to a display. What video interface hardware should be used and what software drivers and/or libraries are available using the Mistral OMAP 35x?
I looked at the OMAP35x Linux PSP Release Notes for PSP 2.00.00.01 it says the framebuffer and v4l2 drivers do not work with DVI.
It also looked like there is Linux Graphics SDK to support OpenGL but it only works with SDK_V1.02 which is an older kernel.
Another source of confusion for me is the processor for this evm is supposed to be OMAP3503 yet the marking on the Mistrel board is OMAP3530 which is another type of OMAP processor. It seems some for the Linux and graphics support one but not the other processor. Is that true?
Can you help?
Thanks
Dick