This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mistral EVM :Problem with minicom



Hi

I'm trying to bring up the Mistral EVM(SAMSUNG NAND).I did following settings.

Selected UART 1(by connecting jumper)

SW4 settings(1-->8 10010000)

Connected UART1 to host(ttyS0) with 115200,8n1 no flow control

but when powered up i dont see anything on minicom console .

On the board i see that lcd is up and demo application running.

i'm sure that null modem cable is fine as it works for other boards.

is my serial port not working or Am i missing something.