Other Parts Discussed in Thread: OMAP3530
Hello,
I'm a newbie to Linux and the OMAP3530 and am trying to debug a simple 'hello world' program (with an additional dummy function called check( ) )on my Mistral OMAP3530 target using the ddd debugger. Here are the steps I'm following:
- Copy ‘gdbserver’ to ~/workdir/filesys/usr/bin
- Build ‘hello.c’ as ‘arm-none-linux-gnueabi-gcc –c –g –o hello.o hello.c
- Restart EVM
- Run ‘gdbserver 192.168.1.100:1000 hello’ from ~/workdir/filesys/opt/hello/hello.o
- On host run ‘ddd –debugger arm-none-linux-gnueabi-gdb ~/workdir/filesys/opt/hello/hello.o
- (gdb) b main
- (gdb) b check
- (gdb) target remote 192.168.1.10:1000
warning: Unable to find dynamic linker breakpoint function. GDB will be unable to debug shared library initializers and track explicitly loaded dynamic code. 0x400007c0 in ?? ( )
- (gdb) cont
warning: .dynamic section for "/lib/libc.so.6" is not at the expected address (wrong library or version mismatch?) Error while mapping shared library sections:
/lib/ld-linux.so.3: No such file or directory
I wasn't sure what these warnings are about and would appreciate any guidance if I need to make any changes to avoid these issues.
Thanks!!