This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Running Demo via ddd on EVM OMAP L-137



I am trying to go through the debugging exercise on the EVM OMAP L-137 via ddd. Is there any document like SPRAAP9 for the EVM OMAP L-137?

That would help me a lot. Or other similar documentation

Thanks,

Davidz

  • SPRAAP9 is geered to UNIX based remote debuging which should work fine on the L137 dev card.  That of course assumes you've allready got linux running on the board.

    if you do not,

    I would look here    

    http://community.ti.com/forums/t/3748.aspx

     for the quick steps.

     

    and there is also a wiki here

    http://wiki.davincidsp.com/index.php?title=Category:OMAPL1

    Which has some good information as well

     

    ~JM