Other Parts Discussed in Thread: OMAP3530
My company is engaged in a consulting capacity designing a system based on the TI OMAP3530 for a client. We originally planned to use the CUS package, but have switched to the CBC package and have uncovered a significant number of discrepancies in the documentation. We would appreciate clarification on these as soon as possible. All the questions relate to the latest version of the OMAP3530.pdf (08 Dec 2008) available on the TI website.
p93 gpmc_d0 AA1 ;AA2 - see p78
p100 i2c3_scl C2 ;i2c2 and i2c3 switched - i2c2_scl - see p80
p100 i2c3_sda C1 ;i2c2 and i2c3 switched - i2c2_scl - see p80
p100 i2c2_scl AB4 ;i2c2 and i2c3 switched - i2c3_scl - see p80
p100 i2c2_sda AC4 ;i2c2 and i2c3 switched - i2c3_scl - see p80
p103 mm3_rxdm AE3 ;K3 - see p84
p105 hsusb1_data7 AA7 ;AA3 - see p83
p108 etk_ctl AB2 ;AB3 - see p83
p108 etk_clk AB3 ;AB2 - see p83
p110 rsv01 AH20 ;No such pin on the 515 pin package
p111 gpio_21 AA2 ;AD2 - see p83
p112 gpio_75 AD24 ;missing from multiplexing characteristics table starting on p76
p114 gpio_137 - ;M3 - see p84
p114 gpio_138 - ;L3 - see p84
p114 gpio_139 - ;K3 - see p84
p114 gpio_140 - ;P3 - see p84
p114 gpio_141 - ;N3 - see p84
p114 gpio_142 - ;U3 - see p84
p114 gpio_143 - ;W3 - see p84
p114 gpio_150 - ;W2 - see p84
p114 gpio_152 - ;V3 - see p84
p114 gpio_153 - ;U4 - see p84
p114 gpio_154 - ;R3 - see p84
p114 gpio_155 - ;T3 - see p84
p116 cap_vdd_wkup NA ;CBB package has pin allocation, surely CBC should also?
p117 pop_ddr_vdd_ft AF13 ;same pin allocated to next signal below on p117 - pop_flash_vpp_ft
p119 pop_reset_rp - ;CBB package has pin allocation, surely CBC should also?
In most cases, we believe that we have resolved the discrepancies correctly ourselves, but it is quite disconcerting to find this many mistakes still present since the initial document release in February 2008. We are in the process of finalizing the schematic for our processor module and need to be sure that we get the pin allocations/signal names correct.
We would like to resolve the discrepancies as soon as possible.
Thank you