Hi all
My job is to make the code as to xdm compliance. I studied all the docs and examples present in dvsdk.
Based on this examples i am writing a simple program that call the ALG_create .
In ALG_create funcion algNumalloc and algAlloc functions not returning anyting eventhough i defined in the library.(processor is going to infinite loop).
1. Lib and Applicaion should point to same include directory path?
2 .Any other examples such that both lib and application in same project(with source code)?
Thanks in advance
suresh