This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beaglebone Black LCD

Hello every1,
We have followed the procedures as mentioned in the website http://beagleboard.org/Getting%20Started#update to boot the OS we are not facing any problem with booting up its working well. 
In order to use the LCD we have disabled HDMI also .
The LCD which we are using is a 5.7" LCD with 16bpp RGB interface mode. 
We have made some changes to the existing device tree give for "cape-bone-LCD3-00A0.dts". 
We are able to set all the required parameters to LCD interface like Pixel Clock, HSync, and VSync we are getting proper output on this pin, only issues is that the Data Enable (DE) signal its not coming properly, so we are not very sure the OS is actually transferring the data to LCD are not,
Can I know the reason for this and also solution for this.
Thank you.