This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Omap35x boot up problem



Hi

I have started working on an Omap 3530 mistral board,  I have been facing problem with the boot up using MMC card.  The board seems to boot up fine with WinCE bootup image which includes MLO, nk.bin and Eboot, however the board does not start booting with Linux the SD card led is lit, I have followed the necessary step which include creating a FAT32 and ext3.  The bootup images mlo, u-boot.bin and uImage on the FAT32 section and the file system in ext3 partition.

Switch SW4 settings which I have tried are:

10011100 (1-8)

01100111 (1-8)

serial ports used :

Uart3

Uart 1/2

File permissions:

-rwxr-xr-x 1 root root  16908  Feb 19 18:15 mlo

-rwxr-xr-x 1 root root 160608 Feb 19 18:15 u-boot.bin

-rwxr-xr-x 1 root root 1929500 Feb 19 18:15 uImage

Kindly provide suggestions.

Thanx