This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems running Codec Engine examples in DVSDK

Hi,

While running codec Engine examples... (Video_copy) I am running into following errors.

1) In loadmodules insmod cmemk.ko phys_start=0x88000000 phys_end=0x8A000000 pools=20x4096,10x131072,2x1048576

Whether the physical start address and physical end address is correct or not?

2)

[root@OMAP3EVM demo_display]# ./app.out

App-> Application started.

[DSP] @0x00000180:[T:0x00000000] servers.video_copy.evm3530 - main> Welcome to 0().

CEapp-> Allocating contiguous buffer for 'input data' of size 1024...

CEapp-> Allocating contiguous buffer for 'encoded data' of size 1024...

CEapp-> Allocating contiguous buffer for 'output data' of size 1024...

Bus error

why we are getting this bus error? we are using the latest versions of codec engine and DVSDK ( codec_engine_2_20_01, dvsdk_3_00_00_29 ).

3) Some times it is getting hung and some times i am getting the following error.

[root@OMAP3EVM demo_display]# ./app.out

App-> Application started.

@0x0004153a:[T:0x40964490] OP - Processor_create_d> Loading and starting DSP server 'video_copy.

@0x0004164c:[T:0x40964490] OP - Processor_delete_d> Closing remote transport FAILED, status=0x80.

@0x00041689:[T:0x40964490] OP - Processor_delete_d> Stopping DSP FAILED, status=0x80008002

@0x000416c6:[T:0x40964490] OP - Processor_delete_d> Closing pool FAILED, status=0x80008000

@0x000416e5:[T:0x40964490] OP - Processor_delete_d> Detaching from DSP FAILED, status=0x80008000

@0x00041816:[T:0x4001cfb0] CE - rserverOpen: can't start 'video_copy.x64P'; Processor_create faid

CEapp-> ERROR: can't open engine video_copy

App-> Application FAILED.

can anyone let me know why this is happening so?

 

Thanks and Regards,

M.BHARATH