This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EDMA3 driver and RMAN works together

Hi, I have a question

I want to use EDMA3 Driver and RMAN for encoder and decoder on C6678 DSP.
The EDMA3 driver uses edma instance #0.
The RMAN configured to use edma instance #1 or #2.

I have added META.createRMObj = false; setting to app.cfg and initialize RMAN after EDMA3 driver.

A kernel crash occurs when one of decoder is initializing.
As I understand, the RMAN uses own functions for creating semaphores, instead of my realization for EDMA3 driver.

So can I use EDMA3 driver and RMAN together?