This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to set fb1 to DVO2 output ?

Hi all,

     I am using RDK4.0. I want to set fb0 to hdmi and fb1 to dvo2. And I can see hdmi was normal but nothing can see at dvo2. Also I use the command to check it out then find that the data was written into fb1.Why nothing out in dvo2?

 Thanks!

Best regards!

The operation:

dd if=/dev/fb0 of=/mnt/userUbifs/fb0dump bs=1 count=50000

dd if=/dev/fb0 of=/dev/fb1 bs=1 count=50000

dd if=/dev/fb1 of=/mnt/userUbifs/fb1dump bs=1 count=50000

compare fb0dump and fb1dump and find that they are the same.