Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO
Dear all,
I would like to know, if there is a (serious) chance to get an OMAP-L137 working without the EValKit.
The reason for this question is the following:
I just want to get a feeling for the OMAP-L137 series , since it might be a perfect solution for a future project. Of course, the costs of such an evalKit are too high for just "playing around" ;-)So i would try to build a quite rudimentary OMAP application. But if i understood the facts presented on the homepage, it is only possible to develop code for the Device over the CCStudio, which (also the eval version) runs only with the dedicated hardware(eval board?)
So: Is there a possibility to program the device for testing small applicatin programs if i don´t have the eval board (and instead of that an own-build board)? [:)]
Thanks in advance for all helping answers and kind regards,
Franz