This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Spectrum Digital OMAP-L137 EVM Software Setup.

Other Parts Discussed in Thread: DA8XX, OMAP-L137

1) According to EVM documentation, this board appears to be considered "similar" to a DA8xx board with reference to the Linux kernel setup.

The SW EVM support released only a  da8xx_defconfig for make kernel configuration.

Is it possible to get a specific  .config file matching exactly the hardware resources of OMAP-L137 EVM ?

2) By means of make xconfig I could myself enable specific driver support for WinBond Spi Flash chip.

Still, I cannot map the Flash chip ranges according to my wishes...

Some specific MTD kernel .config setups ?

The Kernel command line mtdparts setup is OK ?

Thank you for your attention.

 

Uncompressing Linux.................................................................................................................... done, booting the kernel.
Linux version 2.6.18_pro500 (root@plutone) (gcc version 4.2.0 20070126 (prerelease) (MontaVista 4.2.0-3.0.0.0702771 2007-03-10)) #1 PREEMPT Mon Jan 26 14:41:56 CET 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DA8XX EVM
Memory policy: ECC disabled, Data cache writethrough
DaVinci DA0800 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
Built 1 zonelists.  Total pages: 16384
Kernel command line: console=ttyS2,115200n8 noinitrd rw root=/dev/nfs nfsroot=192.168.1.70:/mnt/OmapRd ip=dhcp mem=64M mtdparts=m25p80:8K(DSPAIS)ro,24k(UBL)ro,64k(UBoot)
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 64MB = 64MB total
Memory: 61184KB available (2980K code, 580K data, 156K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 128 gpio irqs
Generic PHY: Registered new driver
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
JFS: nTxBlock = 478, nTxLock = 3825
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c42000 mem 0xfec42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfed0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO map 0x1d0d000 mem 0xfed0d000 (irq = 61) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
Davinci EMAC MII Bus: probed
MAC address is 00:0e:99:02:f4:6e
TI DaVinci EMAC Linux version updated 4.0
i2c /dev entries driver
Creating 3 MTD partitions on "Windbond spi nand flash":
0x00000000-0x00020000 : "U-Boot"
mtd: Giving out device 0 to U-Boot
0x00020000-0x00024000 : "U-Boot Environment"
mtd: Giving out device 1 to U-Boot Environment
0x00024000-0x00400000 : "Linux"
mtd: Giving out device 2 to Linux
dm_spi.0: davinci SPI Controller driver at 0xfec41000 (irq = 20) use_dma=1
dm_spi.1: davinci SPI Controller driver at 0xfee12000 (irq = 56) use_dma=1
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 2 ports detected
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver libusual
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Waiting for PHY clock good...
musb_hdrc: USB Host mode controller at c48a0000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
usb usb2: configuration #1 chosen from 1 choice
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
rtc-da8xx rtc-da8xx.0: rtc intf: proc
rtc-da8xx rtc-da8xx.0: rtc intf: dev (254:0)
rtc-da8xx rtc-da8xx.0: rtc core: registered rtc-da8xx as rtc0
rtc-da8xx rtc-da8xx.0: TI DA8xx Real Time Clock driver.
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc-da8xx rtc-da8xx.0: setting the system clock to 2000-01-13 09:12:27 (947754747)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.126
IP-Config: Complete:
      device=eth0, addr=192.168.1.126, mask=255.255.255.0, gw=192.168.1.2,
     host=192.168.1.126, domain=intranet, nis-domain=(none),
     bootserver=0.0.0.0, rootserver=192.168.1.70, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.70
Looking up port of RPC 100005/1 on 192.168.1.70
VFS: Mounted root (nfs filesystem).
Freeing init memory: 156K
INIT: version 2.86 booting
0
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
Activating swap...done.
Remounting root filesystem...done.
Starting mounting local filesystems: mount none on /var/run type tmpfs (rw)
none on /tmp type tmpfs (rw)
Setting up networking ....
Starting hotplug subsystem:
   pci
   pci      [success]
   usb
   usb      [success]
   isapnp
   isapnp   [success]
   ide
   ide      [success]
   input
   input    [success]
   scsi
   scsi     [success]
done.
INIT: Entering runlevel: 3ortmap
Starting internet superserver: inetd.

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)

192.168.1.126 login:...