This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 IPNC RDK3.5 using tvp5158

Other Parts Discussed in Thread: TVP5158

Hello

I have some questions that used IPNC RDK3.5 and want through TVP5158 multi-ch capture.

I revise m3vpss Firmware, cancel codes about ISS, return Vps_tvp5158Init(), and successfully input it to M3.

At the same time, I revise the multich_usecase’s example “capture_display.c”, "capture" replace "camera".

(Please refer to the attached source.txt)

When it running has some problems as follows:

 

[host] 189: MCFW : CPU Revision [ES1.0] !!! 
[host] 189: MCFW : Detected [4x TVP5158 VS] Board !!! 
[host] 189: MCFW : Base Board Revision [REV A] !!! 
[host] 189: MCFW : Daughter Card Revision [REV A] !!! 
[m3vpss ] VPS_DCTRL_INST_0
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_DVO2
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_HDMI
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_SD
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_HDCOMP
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_CLK_SRC VPS_DC_VENC_HDMI | VPS_DC_VENC_HDCOMP
[m3vpss ] HDCOMPCLK
[m3vpss ] #### (links_m3vpss/capture/captureLink_tsk.c:CaptureLink_tskMain:261)
[m3vpss ] #### (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvCreate:710)
[m3vpss ] 36172: CAPTURE: Create in progress !!!
[m3vpss ] #### Create global VIP capture handle (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvCreate:776)
[m3vpss ] #### CAPTURE_LINK_TMP_BUF_SIZE (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvCreate:785)
[m3vpss ] #### IOCTL_VPS_CAPT_RESET_VIP (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvCreate:795)
[m3vpss ] #### (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvCreateInst:286)
[m3vpss ] #### (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvInitCreateArgs:2114)
[m3vpss ] 36210: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!! 
[m3vpss ] #### (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvIsDataFormatTiled:2093)
[m3vpss ] #### (links_m3vpss/capture/captureLink_drv.c:CaptureLink_drvIsDataFormatTiled:2093)
[m3vpss ] 36210: Assertion @ Line: 677 in links_m3vpss/capture/captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!