Hi,
I'm working on TI EHCI usb remote wake up. something confused me, I want someone can tell me more information.
This device has a ULPI chip(SMSC3320). Usb device connected to device via the PHY.
When the device suspends, the device also suspends. remote wake up is enabled. but when the usb device wakes up, the device can not wake up. but I can see the system's current increased to 170mA.
SO, I think, the OMAP must do something, but can not wake up the system. I turned on the debug option, but no message can be read.
Is there any way that can wake up the device?
BTW, EHCI has a problem to communicate. If there is no usb device connected to USB port. when system suspend, the PHY can not enter into low power mode. I forced it into low power mode, but can not wake up.