This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McAsp Pinmux challenge (9 pin configuration)

Ran into an IO Set Violation and seems like the config I want to make seems impossible. 

The setup we want is a DAC, ADC and DIR, all slaves and connected to McAsp0. (mcasp1 is buzy)
Clocks are 2x external xtal's and goes to ahclkx & ahclkr (as well as to SCK pins on the DAC & ADC).
Bit-clock and frame-sync is shared for ADC and DIR
DAC has it's own frame & bit lines so we can run it in another sample rate.

Below is a list of the pins required (9 in total)

AHCLKX
ACLKX
FSX

AHCLKR
ACLKR
FSR

AXR0 
AXR1
AXR2
or AXR3 

Any McAsp/I2S/pinmux wiz-kids out here? Any help would be greatly appreciated!