Hi,
I have a Mistral solutions OMAP3530 board and a XDS510PP jtag Emulator(From digital Spectrum).
When I try to configure the board in "CCStudio Setup", using the specific configuration
for the mistral board (which is included with the XDS510PP drivers), it gives an error:
"Error automatically generating board file. An invalid router family was specified".
I am Using Code_Composer_Studio_v3.3_Build_3.3.38.2_FET and setupCCSPlatinum_v30329 drivers from Spectrum Digital.
Did anyone come across this error?
Please Help
Regards
Jack