Hi all,
I'm trying to use the viddec3test application with KMSCUBE display, but I have no luck at the moment. I'm able to run the kmscube aplication and I'm able to decode a video using the viddec3test application, but when I try to use the kmscube display i doesn't work.
The command I use is the following:
viddec3test --kmscube myvideo.mov
And the error I finally get :
ERROR:decoder_process:390: 0x1b070: process returned error: -1
ERROR:decoder_process:391: 0x1b070: extendedError: 00000000
ERROR:decoder_process:318: 0x1b070: fail: out of buffers
Segmentation fault
I tried with different video formats and diferent video sizes.
There is something special to do in order to run the viddec3test application with kmscube ?
Regards,
Enric