5047.applyTableBinitCmdFile.txtAll:
I have encountered a script file that has some comments:
"This is a snippet of the DSP/BIOS generated linker command file,
Before the function call
.bios: {} load > FLASHREST, run > IRAM
After the function call
.bios: {} load > FLASHREST, run > IRAM, table(BINIT)"
Obviously very useful if you are moving something from Flash to Ram via bootloading mechanism. Is this a TI-generated file? Can it be ported from the CCS3.3 environment to the CCS5.5 environment?
BTW, at the end of the file is revision history of
18-Jun-2004 alancam Created
If this file can be used with CCS5.5, can it be altered to have the MEMORY { } excluded, so that I do not get a doubly-defined memory when I include the Bios-generated cmd file with a customer cmd file?
I have attached the .tci file as a .txt file.