This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to set Dynamic targetBitRate of Enc_Link using Venc_setDynamicParam?

Hi All,

I was working on IPNC_RDK 3.5 version. when I try to set targetBitRate as dynamically
using Venc_setDynamicParam API, the below error message i was getting.
   

This Venc_setDynamicParam(1, 0, &params, VENC_BITRATE); API I was calling after Venc_start()
function.

Error Message

----------------------------------------------------------------------------------------------------------------------------------------------------

 [m3video]  ENCLINK: new targetbitrate to set:4000
 [m3video] 14093:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[191]::INTERNAL ERROR:-1
 [m3video] ALGCONTROL FAILED:CMD:1
 [m3video] ERROR: XDM_UNSUPPORTEDPARAM = 14,
 [m3video] ERROR: XDM_FATALERROR = 15
 [m3video] ERROR: IH264ENC_UNSUPPORTED_VIDENC2DYNAMICPARAMS = 30,

 [host] Error code: -1 at 440
 [m3video] 14094:WARN
 [m3video]  ENCLINK: ERROR in Run time parameters changes, Extended Error code:1073790976
 [m3video] Extended error 4000c000 for reqObjIndex 0

--------------------------------------------------------------------------------------------------------------------------------------------------------



can anyone please clarify the way I have done is proper way? and what is the root cause
of this issue?

please suggest me to fix this issue.

Thanks in advance

Regards,
Kolanchi.