Hi all,
Our requirement is to display video in HDMI display and stream the same through RTP with RTSP server.
I have compiled RTSP server for Gstreamer and integrated with EZsdk and written a sample application to initialize the RTSP server session. RTP/RTSP streaming is working fine.
Now the issue is I can see video in HDMI display only once any of the client made PLAY request for RTP stream through RTSP server.
I am giving following pipeline to the RTSP server.
"omx_camera input-interface=VIP2_PORTA ! video/x-raw-yuv, format=\(fourcc\)NV12, width=1920, height=1080, framerate=\(fraction\)60/1, buffer-count-requested=10 ! tee name=t ! omx_scaler ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! omx_videosink sync=false t. ! omx_h264enc ! queue ! h264parse ! gstperf ! rtph264pay name=pay0 pt=96 "
I should be able to get video in HDMI display even if nobody request for RTP stream.Please help me to find a solution for this.
Thanks,
Abeesh