One of the customer is facing the following problem,
" We procured OMAP3503 EVM. we tried to connect the evm 3503 target but it is showing problem. we are using spectrum digital emulator for this.Emulator is working fine.while connecting to target,ARM CORTEX Processor was connected but DSP Processor is not connecting. It is showing the following error message " Target does not have CPU Clock".
"
I remember that OMAP platforms, requires the DSP to be clocked and reset first from ARM through GEL.
Then only one can connect to DSP.
Can some one point to the right set of steps and the GEL files.
Thanks and Regards,
Venu